AXIS#.IL.DIFOLD

Description

AXIS#.ILClosed "Instruction list" This is a low-level language and resembles assembly.DIFOLD is the output of the drive foldback algorithm. It is an artificial current which is always above the drive continuous current, AXIS#.ICONT . When AXIS#.IL.DIFOLD is lower than AXIS#.IPEAK, it becomes the active current limit.

AXIS#.IL.DIFOLD decreases when the actual current is higher than drive continuous current and increases (up to a certain level) when the actual current is lower than drive continuous current.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

0 to 2,147,483.647 Arms

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.DIFOLD 0x500A 0x7 DINT 1000:1 - RO False
AXIS2.IL.DIFOLD 0x510A 0x7 DINT 1000:1 - RO False